This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61185: TPS61185 Frequency Program PWM Dimming

Part Number: TPS61185


Hi,

We got a questions from customer about TPS61185.
Could you help us?

[Question]
They measured PWM dimming frequency in frequency program PWM dimming by EVM. The result is below.

 Vin=10.8V
 LED=8S4P
 Riset=56k

They think PWM dimming frequency is poor accuracy at Rfpwmo=100k. Why is it poor accuracy at Rfpwmo=100k?

Best Regards,
tateo

  • Hi Tateo,

    Sorry for the delay. I've asked the design team to get clear information.
    Please let me share if any update.

    Best regards,
    Milo
  • Thank you for your reply.
    Please let us know if you get the feedback.

    By the way, we got additional question.

    - How much is the minimum PWM input ON time?
      My customer should be specified 1% Duty at 20kHz PWM input frequency by frequency program PWM dimming. They have consern about the PWM input minimum ON time.

    Best Regards,
    tateo

  • Hi,

    according to the datasheet pg15, the minimum on time in each dimming cycle is 5us, which means the minimum duty of PWM dimming can reach down to 1% when dimming freq is less than 2KHz.

  • Thank you for your reply.
    PWM input minimum on time and PWM dimming minimum on time are same value that is 5usec. So when they use frequency program PWM under the following condition, minimum PWM dimming Duty is 10%. Is it right?

     - Condition -
     PWM input frequency=20kHz
     Rfpwmo=100kHz(PWM dimming frequency=1.5kHz)

    And please give us your feedback about first question.

    Best Regards,
    tateo

  • Hi Tateo,

    For dimming frequency setting, the integrated oscillator need to be trimmed to ensure the accuracy. We could only trim the oscillator at one condition. The 210Hz is quite popular dimming frequency when we were designing TPS61185, so we trim the frequency at 210Hz. So the accuracy for dimming frequency will be good at 210Hz and worse at higher frequency. In the other hand, I would suggest customer to use 210Hz for dimming frequency instead of 1.5KHz, because 1.5kHz is in sensitive audiable frequency range and the acoustic noise on ceramic capacitor at this frequency is much easier to be heard.

    Best regards,
    Xianghao
  • Thank you for your support.
    Please let me confirm your answer about PWM input minimum on time.

    PWM input minimum on time and PWM dimming minimum on time are same value that is 5usec. So when they use frequency program PWM under the following condition, minimum PWM dimming Duty is 10%. Is it right?

    - Condition -
    PWM input frequency=20kHz
    Rfpwmo=100kHz(PWM dimming frequency=1.5kHz)

    Best Regards,
    tateo

  • Below is recommended application conditions in datasheet.

    The minimum 5us Ton is only for FPWMO. So i think the minimum PWM dimming duty is 1% for PWMIN=20kHz and PWMO=1.5kHz.

    BEst regards,

    Xianghao