I have seen from previous threads that enabling IT before pack assembly is not recommended due to the potential for introducing errors into the Gas Gauge function. It Was also mentioned that changing the Update Status from 06 to 02 (disabling IT) would not clear up the problem. However it was also stated in the same thread that most errors introduced would be worked out over the first few charge/discharge cycles.
My question is this: I have 130 newly manufactured packs that had the Update Status erroneously set to 06 in my .rom file when they were programmed/calibrated via MultiStation tester. The packs have not yet been software sealed. Can the issues with the wrong Update Status be resolved by issuing a System Reset (0041 command) before re-enabling IT (0021 command)? This would be preferable to having to go back and manually re-program all 130 units (load default .senc file, load new .gg file, recalibrate V,T,I, and offsets, then reset and enable IT).