This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27542-G1: Device reporting Wrong SOC

Part Number: BQ27542-G1
Other Parts Discussed in Thread: BQ24190, CC3200, BQSTUDIO, EV2400
We are having an issue on the IOT devices reporting wrong SOC even though the battery does charge completely. This started happening on a handful of devices since past 2 weeks and we are using the fuel gauge BQ27542. So the SOC does get updated correctly for a certain period of time e.g. 0 to 73% and then it stays on 73% after that. When I checked the voltage on the battery it says 4.2V which is completely charged. 
So I just wanted to ask why after a certain period of time the same fuel gauge did start reporting the SOC incorrectly? These devices were running same hardware for past 6 months and were reporting the SOC correctly. 
I am using CC3200 as the master device to program the gauge. I feel somehow firmware update might have changed the coordination between charger IC and fuel gauge. The charger IC is BQ24190. The battery is rechargeable Li-ion. Any comments/help would be appreciated.