This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM53600-Q1: Light load efficiency of LM53600-Q1

Part Number: LM53600-Q1
Other Parts Discussed in Thread: LM53601-Q1

Dear support team

My customer want to actual effiency data of light load.

Could you provide it ?

◆LM53601-Q1

Vin=12V,16V,8V Vout=3.3V Iout=100uA (PFM mode)

Regards

Tomohiro Nagasawa

  • I can give you approximate typical values for efficiency as follows:

    8V: 58%

    13V: 46%

    18V: 39%

    These values are for reference only and do not necessarily represent the best performance of the device, nor what the customer can expect.