Hi everyone,
I'm trying to choose my battery charger (and fuel gauge to monitor de capacity, but I'm going to leave this issue aside for the moment).
1º.- So first of all, I need to choose the battery I'm going to use. The application is a portable device with a Li-Ion battery of 5000 mA, so If I choose a charger capable of supplying around 2A, It takes me around 3,5 hours to charge the battery, I'm right?
2º.- I know the voltage input to charge the battery is going to be 5 Volts DC. And system output has to be between 3.3Vdc - 4.2Vdc.
3º.- Now, I need to choose from a switch-mode vs a battery charger. I know the benefits of a switch-mode, they minimise the power dissipation but consume more space in PCB than the linear chargers, as well as, the switch-mode charges are noisier than linear chargers but at the same time, I need to be careful with EMI because I need to certificate the final product, so for this issue it'll be better a linear charger.
But in my case, I need to charge a 5000 mA battery, so I need to charge the battery in around 4h, so I'm going to need a high rate current so If I use a linear charger is going to heat a lot (I remember that I'm going to use an input voltage of 5V, so I don't have experience if the system is going to heat too much or not. Anyone has checked something similar), and the heat is bad for batteries and electronic in general.
I would like that the charger was self-sufficient, that it's to say, I don't need an i2c port to configure any setting. I would like that charger was able to be connected to any typical charger, similar to the phone chargers.
Any suggestion?
Best regards.