This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2H160-Q1: About 2ch in parallel

Part Number: TPS2H160-Q1


Hi,

I would like to know it is possible to use as 1ch switch be connected in parallel ch A and B.

I am looking for 1ch high side switch.

I am assuming the nominal current is 1A and maximum continuous current is about 2.5A.

The ambient temperature is up to 125 degree.

I am relieved If it will be lower the on-resistance.

Best regards,

Tomoaki Yoshida

  • Hi,

    It is possible to parallel the channels together. The challenges you will run into are with the diagnostics that are meant for one channel or the other.

    I would also recommend the TPS1H100 device as well since the diagnostics are optimized for a single channel operation.