Part Number: TPS65560EVM-165
Hi
I bought one of these development boards a couple of years ago but this is the first time I've fired it up.
Basically the Xenon lamp is not flashing. I can charge the cap to 320V I get a flash full signal to the led.
I can trigger using the switch and get signal all the way through to the IGBT. I can see that the IGBT is firing. The voltage between C6 and R9 is switching.
The lamp partially lights dimly and the charge voltage drops about 10v.
Any suggestions ? lamp or trigger transformer maybe ?
Thanks
David