Other Parts Discussed in Thread: LM5022
We are using the TPS40170 in a flybuck converter (10-60V in, 3.3V 5A out). Our problem is the correct values for the Ilimit resistor: Setting it to the requested current limit (5A) it works fine during normal operation, but does not startup (SS cap 100nF). The current limit resistor has to be set for 12A continued operation to allow the startup. At a lower value several softstart cycles are necessary to achive the stable operation.
Trying to understand we looked at the datasheet SLUS970B. It is recommended the TRK pin is tied to the VDD if not used, but section 7.3.7 says "For proper tracking using the TRK pin, the tracking voltage
should be allowed to rise only after SSEAMP has exceeded VREF, so that there is no possibility of the TRK pin voltage being higher than the SSEAMP voltage". Maybe it is not OK to connect the TRK to VDD and that generates the softstart not working as expected, generating overcurrent switch off?