This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ51025: Component Values for 5 Volts at 2 Amps

Part Number: BQ51025

Hello team,

I am supporting an application using the bq51025EVM-649 that is setup for 7 V and 1.4 A max, we would like to test it at 5 V and 2 A, but there has been troubles with the results after changing the current limit.

Would you be able to share the optimized component values for the entire circuit with an output of 5 V at 2 A?