Other Parts Discussed in Thread: TPS61071
Hello Team,
I am working with a customer who is looking for a DC/DC Boost Converter for their current application. Below are the requirements for the boost converter:
Input Voltage: 2.4V typical
Output Voltage: ~5V
Output Current: ~300uA (very low)
Initially, the customer is looking into the TLV61220 boost converter, and had a question on the inductor size limitations.
After reviewing equation (2) in section 11.2.2.2 of the datasheet (seen below), I calculated Fsw to be roughly 1.35MHz when the Iout is 200mA and L = 4.7uH (well above 75kHz).
When I modified Iout to equal 300uA, and L to be 2.2uH (lowest recommended value) the Fsw turned out to be 1,925 MHz. Considering that the switching frequency limits of this device are 500kHz < Fsw < 2,000kHz, this solution is not a viable option. Is there a specific reason why we cannot reduce the inductor below the 2.2uH? I don't foresee that reducing the inductor will be able to put us where we need to be, but I was just curious on the reasoning behind the limitation.
Best Regards,
Javier Palomo