When configuring the VBOOST value in adaptive boost mode, does this value include any headroom? For example, if I set the VBOOST for 30V, does this represent the initial voltage across the LEDs, such that the actual boost voltage relative to GND will be 30V + LED headroom?
Also, why are there two registers to set the LED headroom setting: DRIVER_HEADROOM and HEADROOM_OFFSET? It's clear that the threshold is based on the sum of these settings, but does it matter which settings are used to achieve a particular value?