Part Number: LMG3410
Hi
Our customer are going to use this device. And they are considering the configuration with digital iso.(ISO7831,ISO7821 etc..)
There are two configuration.
1. The digital isolator is used for high side and low side.
(e.g. LMG3410HB-EVM http://www.tij.co.jp/jp/lit/ug/snou140/snou140.pdf
2. The digital isolator is used for only high side.
(e.g. Datasheet Page 1. Simplified system diagram )
Which do you recommend? The cost of #1 will be higher than #2.
Could you give us any advices for each type of configuration if there are any concerns?
We would like to chose the #2 if there are not any concerns.
Regards,
Koji Hamamoto