Hi,
we have an issue with the FullChargeCapacity.
We are setting up the system like this:
1) program the default srec from TI webpage
2) Import the .gg.csv file attached
3) Set the Chemistry to 2012
4) Reset the system (disconnect from cells, power up again)
The problem is the FullChargeCapacity. It is correctly set to the DesignCapacity if the value is queried in mAh. But if queuried in cWh, then the value is not correct. For example we get 140Wh instead of 180Wh. We tried this i few times from the beginning with different settings. It never was set to the correct value. It seemed to be rather random.
What are we doing wrong?
Thanks,
Simon