This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65265: DC DC doesn't start automatically

Part Number: TPS65265

on my board the TPS65265 is configured with MODE = '0' EN1 = '0' EN2 = '1' and EN3 controlled by GPIO, so there is a power-up sequence after EN3 is enabled

after power up nothing is coming out of the three outputs

when changing the strapping to MODE = 'Float' EN1 = '1' EN2 = '1' and EN3 = '1' by resistors the TPS65265 is working properly

did I miss anything?

see attached schematics for more details