This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2623: about step down condition

Part Number: LM2623
Other Parts Discussed in Thread: TPS63070

Hi,

Could you tell me about LM2623?

My customer is looking for a device that meets the following conditions.
-Vin(min): 1.2V ※as minimally as possible
-Vin(max): 7V
-Vout:4.5V or 5V
-Iout≒ 250mA

I introduced LM2623 and TPS63070 to customer.
However,Customer wants an input voltage lower than TPS63070.
Can this device(LM2623) be used in customer's condition?
And,In the case of step down condition, please tell me what operation this device.

Best Regards,
Yusuke/Japan Disty