Tool/software: Webench
Hi!
I have a project that includes Buck-Boost converter TPS63050.
Components:
10uF Capacitor - GRM219R61E106KA12D
1.5uH Inductor - SDE0604A-1R5M
Problem:
-Ripple is too high
-Firt time power up after soldering (PCB was still hot) everthing worked correcty with good ripple, voltage and current. (with load 50ohm and no load)
After trying some diffrent test I notice increase in current (400mA but still 3.3V-3.5V) and at that point TPS acted weird. For me it is strange because I checked inductor, capacitor and layout five times. I even try to replace TPS and result was same. Strange thing is TPS works correctly only when board is warm (hot).
Please tell me what could be the problem. (Was soldering with hot air, maybe i destroyed both chips?)