Other Parts Discussed in Thread: BQ34Z100-G1, BQSTUDIO
Hi,
The datasheet for the bq34110 says that Rsense should be between 5 and 20 mOhms. However, the app note slua792 tells that it's not really a problem. Are there any problems with increasing the Rsense to get a better LSB for the CC ADC?
For example, I got that the worst LSB (when ADC is 14 bits, not 15) in volts of the device is:
LSB = V(SR) / 2^14 = 0.25 / 2^14 = 15.259uV
If I want a current LSB of 50uA, I need to have a Rsense of 305.18 mOhms. This sets my maximum readable current to:
I(max) = V(SR) / 2 / Rsense = 0.25 / 2 / 0.305 = ~410mA
This maximum current is perfectly fine for our application. Except for a higher dissipation at Rsense, are there any reasons why this Rsense value wouldn't be acceptable?
Thanks,
Fred