This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2776: LM2776 EN pin input structure and input current

Part Number: LM2776

Dear Members

Could anybody please comment on the following?

1) Is the EN pin internal pulled up to the input supply by a weak current source (probably not)

2) Is there any data available as to the input current of this pin (min, typ, max)?

Thank you