Referring to the data sheet for the TPS74401, section 6.3 Recommended Operating Conditions shows a maximum Vbias of 5.5V while the Electrical Characteristics section 6.5 shows a maximum Vbias of 5.25V. Normally this might be irrelevant except that I'm trying to set Vbias at 5.36V. I'm not picking up what the distinction is between these two limitations.