Hi,
With reference to the statement below and the LM5050-1 datasheet, my understanding is that the "OUT" pin is just for protection means by sensing the voltage on the drain pin. If I donot want to use this pin and leave it no connect, my understanding is that gate voltage will be clamped to max 12V above the source/ IN pin to turn ON the fet. Is my understanding correct or am I missing something.
In forward operation, the gate of the MOSFET is charged until it reaches the clamping voltage of the 12-V GATE to IN pin Zener diode internal to the LM5050-1