At first glance, beside a larger regulated voltage error that assumed, everything’s seem to work fine as the circuit can drive various load without problem but when I look at the frequency at which the SW pin toggle, it is around 362kHz instead of more than 1Mhz as I choose an RT resistor of 68k. Moreover, I just remove that RT resistor and the frequency did not change at all! Could it be a bad controller? When I look at the signal on pin RT/CLK what I should see?