Other Parts Discussed in Thread: BQSTUDIO
I am designing a portable instrument that is powered by 4 series LiPo cells producing 16.8 V. The cells are 9000 mAH. My requirement does not require rapid charge or discharge of the cells. My maximum discharge current is about 300 mA. I need to charge the cells in about 12 hours. The large cell capacity is to permit the instrument to operate in the field away from charging power for an extended period.
My question is can the bq40z60 charge the cell stack from 13.75 V cigarette lighter socket or must I implement a voltage boost circuit if charging from a car battery is needed in an emergency. Normally the instrument would be charged from an AC to DC p[owerr module at the operations base.