This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22990: Is there a maximum CT(pF)/output rise time spec?

Part Number: TPS22990

Hi team,

In datasheet, the maximum CT cap is up to 10,000pF (10nF) and output rise time is up to 598.5us (VIN = 5V). 

I would like to know if CT cap can be increased to, say ~200nF in order to increase output rise time to ~10ms+? 

Thanks!

  • Hi Pengyu,

    The CT capacitor does not have a maximum value, but exceeding the table limits may cause concern from a thermal perspective depending on the loading conditions. In your application, what is the load capacitance and load current on the output of the TPS22990?

    Thanks,

    Alek Kaknevicius