BQ40Z60EVM has a series resistor 10kOhm at ACP pin. I suspect it to be the major source of Vacp measurement error.
Can this resistior be replaced, say, with 1kOhm or less? (Overvoltage protection is not an issue in my case.)
Regards,
Sergey
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
BQ40Z60EVM has a series resistor 10kOhm at ACP pin. I suspect it to be the major source of Vacp measurement error.
Can this resistior be replaced, say, with 1kOhm or less? (Overvoltage protection is not an issue in my case.)
Regards,
Sergey
Hi Haidar,
do you mean 100kOm is an internal resistor in BQ40Z60? Such a divider couldn't guarantee 1Vmax output with 26Vmax input. Data sheet states it a bit differently:
Anyway, I can see neither 40 nor 100. In fact just about 200mV drops at 10kOhm with Vacp=12V, which suggests about 600kOhm internal resistor (if there is any). This dropout varies with time (mode?) and input voltage and likely serves a source of inaccuracy, which I observe. Calibration brings no relief. Meanwhile battery voltages measurements are quite accurate.
Please re-check your information. Of course, if 10kOhm is really an intended value for some reason, I would have to give up.
Regards,
Sergey
RPD |
Internal pulldown resistance | ACP | 30 | 40 | 50 | kΩ |
Above is an extract from data sheet which I unsuccesfully tried to paste directly in the previous post.
Regards,
Sergey
Hi Haidar,
thank you, this explanation seems to have better ground. Nevertheless, as far as I can see, actual behavior doesn't prove this model.
Please consider the below data
Vacp, mV |
Charger enabled |
Charger disabled |
||
Vacp measured |
drop@10k |
Vacp measured |
drop@10k |
|
10003 |
9771 |
203 |
10014 |
25 |
11998 |
11769 |
206 |
11996 |
28 |
14995 |
14770 |
209 |
14973 |
33 |
20045 |
19736 |
216 |
19968 |
40 |
Note: Vacp channel was calibrated at 12V with charger disabled.
This data suggests that major contributor to the drop voltage at 10kOhm resistor is probably charge pump supply current.
As to ACP pin pulldown resistor, it may have been switched off when Vacp present, or at least it should be about 5MegOhm to explain few millivolts drop at 10kOhm resistor with disabled charger.
To have measurements more accurate the drop at 10kOhm resistor should be made minimal (or constant). This is why I ask of possible contra-indications to reducing 10kOhm to 1kOhm or so.
Regards,
Sergey
Vacp |
Charger enabled |
Charger disabled |
||
Vacp measured |
drop@10k |
Vacp measured |
drop@10k |
|
10003 |
9771 |
203 |
10014 |
25 |
11998 |
11769 |
206 |
11996 |
28 |
14995 |
14770 |
209 |
14973 |
33 |
20045 |
19736 |
216 |
19968 |
40 |
Hi Sergey,
Yes you can reduce the resistor to 1k to minimize the drop. The ACP pin is the supply for the internal charge pump (CP) and when it draws current, it results in at voltage drop in VACP. Reducing to 1k minimum will help minimize the drop.