Other Parts Discussed in Thread: BQ24630, BQPRODUCTION, BQSTUDIO
Hi Team,
Can you please comment on the following questions regarding the BQ40z50-R1?
- Please explain the FC, FD, TC, TD functions. They aren’t explained in the TRM and not even mentioned in the datasheet. Is there other documentation that I’ve missed?
- How are the Calibration section parameters set? Or are these set during use, so they don’t need to be programmed on a new pack? In other words, are these parameters part of our factory-installed pack parameter file?
- In the Enabled Protection registers, it would be very useful if for every bit the parameters that will be used if enabled were referenced. I know what I want enabled and disabled, but don’t always know which parameters need to be set correctly when a particular protection is enabled. Most can be found by searching the bit name though, which is helpful.
- If one has a “dumb” charger like the BQ24630, should all charging-relative protections be disabled? For example, bit 7 (CHGC) of Enabled Protections C register and another are bits 0 and 1 of Enabled Protections D register.
- What does “Rec” mean? It pops up a lot, such as “Rec Temp” and other places. Recommended?
Thanks,
Nabeel