Other Parts Discussed in Thread: BQSTUDIO,
Hello gents and ladies.
Im considering to design a battery charger as a university project and came across BQ4050. On the datasheet it is stated that 6A discharge is the default setting for the over discharge protection to kick in. Im required to use bqstudio to change that setting. My design requires 10A continious discharge and 4A charge. I downloaded the bqstudio and it did not run on my PC. Now the question is what are the max limits for over discharge and over charge current parameters? Can i set those settings to be equal and higher than my requirements?
Thank you very much in advance.
Have a great day.
Mr. Orkhan Aliyev.