Part Number: LM2676
Hello,
It's the third prototype I'm designing and the LM2676-5.0 isn't working. I followed the layout guidelines but it is not better. My output is at +/- 7 V... What should I do to get an operational power circuit ?
Component used :
Cin : 4.7 uF + 100 nF
Cout : 100uF
Inductor : 33 uH 2.8 A
Diode : Schottky 60 V 3A