Dear,
I use TPS63020 to convert 3.7V battery to 5v in the medical product. When I test the model, the EMI of it excessive the standard line of class B in IEC 60601-1.
So, there is the problem that
1, if anyone meet the problem while using the chip?
2, In order to pass the test, what should i do if i still want to use this chip?
3, Are there other chip with low EMI that i can use to replace this chip?
Below is the picture show the EMI situation of the TPS63020,