Other Parts Discussed in Thread: BQ25896, PMP11536, PMP4496, BQ25895, BQ24192
Hi,
I have been looking at the BQ24192I charger which I want to use in a battery powered application with only an USB Type-C USB 2.0 connector as the only connector. It has to act as a DRP and be able to be charged according to the advertised capabilities (but 3A max) when ever possible while communicating on the USB 2.0 data path, or it must be able to source (500mA max) a UFP device (memory stick etc.).
If connected to another DRP it shall prioritize the UFP role so that it can be charged.
I would like it to be able to also function without the application processor when the turned off, so that we dont have to boot the device when attaching a charger. When on my device has an application processor with I2C connection.
I have also looked at the BQ25896, but I'm not sure what the differences are.