This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

I am looking forward to design 1 kWh battery pack along with Battery management system using 3.7V, 2.2 Ah Li-ion cells

Other Parts Discussed in Thread: BQ76940

Hi,

I am new to power electronics and design. I am looking forward to design Li-ion battery pack with following specifications. In this regard, I need your help in choosing my Ti parts in various stages.

Input specifications:

Individual Li-ion cell specifications: 3.0V - 4.2V (3.7V is nominal), 2 Ah is capacity.

Battery pack: 14 cells in series , 10 cells in parallel. (48V, 20 Ah).

Design requirements for battery pack with battery charger, battery protection / management:

Maximum charging current is 10A.

Maximum discharge current is 4A.

Charger input: 230V AC.

Charger output: 60V DC, 10-15A current.

(Transformerless AC to DC type Charger design may be considered inview of less weight and size constraints)

For utilizing power from battery pack to utilities, DC to AC conversion is also required if possible in the same design circuit.

Basically, a low weight (probably transformerless inverter type design) DC to AC inverter circuit may be integrated along with battery charger and battery management system.

Expecting support from Ti team.

Regards

Balakrishna.

CSIR, India.