This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LMZ10503: LMZ10503 WEBENCH Designer

Part Number: LMZ10503


Tool/software: WEBENCH® Design Tools

Hi,

I tried to use TI WEBENCH Designer to design a circuit using LMZ10503 with the following specs:

Input voltage range 3V to 5.5V

Output voltage range 4.5V to 5V

Output current 2A or 3A

Ambient temperature 50 C

but the solution is not  available and components not appeared.

can you help me to design it?

Thanks in advance

  • Hello Ahmed, 

    The LMZ10503 is a step-down regulator. 

    In your design specifications you have 3V as your minimum input voltage. The output voltage you specified (4.5V-5V) is higher than the minimum input voltage. The LMZ10503 will not show up as a suitable solution in this case. 

    Cheers, 
    Denislav