This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63050: External driven output with no input present possible?

Part Number: TPS63050

I'd like to integrate a TPS63050 in our design.

However there will occur a situation (during programming of our device) when the IC is not powered but its output is powered externally.

Is this an allowed state for this IC?

The datasheet says that the output is disconnected if the device is disabled but I fear that the 0.8V on the feedback pin might somehow damage the device if no input is present.