Other Parts Discussed in Thread: UCC2897A
Hi Team:
Do we have any solution can support below requirement?
1. Isolated.
2. Input is -36V to -76V.
3. Output is 28V
4. Output current is 3A.(Max)
5. Efficiency is higher than 85%.
6. Ripple is below 1.5%.
I use webech to simulate but the part is UCC38XX family and the efficiency is only around 77%.
Do we have any TI design can refer to? Thanks a lot.