This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A8300: Heat sink attachement

Part Number: TPS7A8300

Hello guys,

I am relatively new to power management design with heat sinks. I use the TPS7A8300 with 6VDC IN and 4VDC OUT@ approx. 1A worst case.

At first I used the TI webench for thermal simulation without a fan and found that with thick copper I am pretty much on the safe side. The problem is, my design has some pretty small ICs so I can't use 105µm thick copper unless I create two PCBs which is not desired. So I resimulated with 35µm copper where the device will heat up too much without a heat sink. Since the TPS7A8300 has thermal pad design I wanted to ask if this will work, if I attach a glued heat sink on the device's top for propper thermal drain, or if this will not work, because the thermal pad is the only way to remove heat from the device.

best regards

Benjamin

  • Hi Benjamin,

    You can add an external heat sink to this device. The following thread discussed how another customer chose to use a heat sink on a similar packaged device:

    e2e.ti.com/.../536997

    Please note that one way to reduce heat (and conserve power in your application) would be to reduce the voltage drop across the LDO. The most efficient way would be to place a switching regulator before the LDO; however, simply placing a power resistor or even another LDO in series before the TPS7A8300 will spread the heat.

    Very Respectfully,
    Ryan
  • Hey Ryan,

    thanks for your fast reply! Sadly chip count and size are really important in the design, and since I have a lot of different Voltages (5V, 4V, 3.3V, 2.7V and 1.35V) I have severeal different devices already. I will stick to the heatsink.

    best regards

    Benjamin