This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A1601-Q1: looking for an LDO with reverse bat protection 36V to 5v 0.1A

Part Number: TPS7A1601-Q1

looking for an LDO  with reverse bat protection 36V to 5v 0.1A

if possible similar package as the TPS7A1601DGN

  • Hi Kamal,

    Our linear regulators with reverse battery protection can be found under the special features "reverse voltage protection." Plugging in some more information from your provided application requirements I found the following 4 results:

    http://www.ti.com/lsds/ti/power-management/linear-regulators-ldo-products.page#p451max=0.1;7.5&p238max=36;125&p2192=Reverse Voltage Protection&p1498=Automotive 

    Very Respectfully,
    Ryan

  • Hi Kamal,

    In addition to the recommendations Ryan put in the link; The TPS7A1601-Q1 alone can not support reverse battery or reverse current. However, we did design the VIN to operate down to 3V so you can put a diode in series with VIN to realized the reverse battery/current protection.

    I hope this helps.

    Regards,

    John