Other Parts Discussed in Thread: TINA-TI,
Tool/software: TINA-TI or Spice Models
Hello, I have two questions please regarding this component.
1) Can I find somewhere the lib for the LM1086 for Eagle/Altium? It seems I need to make my own because it's missing from my libraries and I am not experience with that.
2) I am afraid that my schematics (designed by someone else) are wrong. Please see the following, the regulator is replaced by LM1086, R3 =120 Ohms and R4 = 200 Ohms. The Vin=5V, Vout =3.3 V, Vadj =2 V. It seems that when I plug my power supply on a laptop I see a huge spike in the output ( from -10V to 10V) I believe that this might have destroyed some pcbs. I also see spikes on the outputs of two cameras. As a result, usually one of the cameras is not recognized anymore. Isn't the role of the voltage regulator to provide 3.3 V stable and robust to external disturbances? Could it be that the Rload in the output the designer selected is wrong? Maybe I should replace it with a bigger value and the capacitor at the output as well? How should I choose the cap?
Please make any suggestions if you re more experienced in that. All the components on the pcb are smd. It is hard to measure the cap without removing it and I am afraid I won't re-solder it correctly. Thank you in advance !!!