We are using the LM5170-Q1 for parallel operation.
If 4 modules are operating in parallel, how this IC handle the load balancing on each module?
Is there any application note or details on this?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi David,
Since the LM5170-Q1 is an average current mode controller the current will be shared evenly between each phase. For example if the the total load current is 100A each of the 4 phases will conduct about 25A of current. When comparing average current mode control (ACMC) vs peak current mode control (PCMC), ACMC shares the current more evenly as it has more noise immunity than PCMC.
Figure 9 of the EVM user guide shows how the current is shared evenly between each channel.
Thanks,
Garrett Roecker