Hi Team,
I am considering using BQ24650 for a customer application requiring the following specification:
Battery voltage: 27.3V
Constant current requirement:1.2A
Temperature : 0-80 degrees C
I saw in an other e2e thread that the maximum duty cycle for this chip if you want to keep regulation is 97%. With 28V in input 97% of duty cycle gives 27.2V in output, it could fit but I'm afraid to be too closed to the limits of the chip especially at 80 degrees.
Do you think this chip would fit for this application ?
Thank you,
Bastien