Hi Sir,
If BQ25895 using 5.3V/0.85A solar power input, this source only have power and ground, I just need connect D+/D- together, let it always recognize to 5V/1A input, right?
Thanks!
Jeff
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir,
If BQ25895 using 5.3V/0.85A solar power input, this source only have power and ground, I just need connect D+/D- together, let it always recognize to 5V/1A input, right?
Thanks!
Jeff
Hello Jeff,
If D+/D- are shorted, the D+/D- detection on the bq25895 will detect the connection as DCP and set the input current limit to 3.25A. This will allow the device to use the full 0.85A from your input.
Having said that, if you want to limit the input current limit to 1A, there are two options you can also follow: