Other Parts Discussed in Thread: TPS62400
Hi !
I am using LM26480 and TPS62400 power regulators.
TPS62400 buck 1 provides output = 3.3V
LM26480 Bucks are powered by 5V and LDOs are powered by 3.3V (from TPS62400)
Various supply connections is as follows
AVDD = 5V
VIN BUCK1 = VIN BUCK2 = 5V
VINLDO12, VINLDO1, VINLDO2 = 3.3V (powered from TPS62400)
So , when this setup is powered, TPS62400 voltage shows as 4.2V and its not switching 3.3V output.
When I removed, 3.3V connection from VINLDO12, the 4.2V is gone and TPS62400 starts switching 3.3V out.
Looks like there is a leakage between VIN (5V) to VINLDO12 ? Is it that we have to power VINLDO12 to the same supply as AVDD ? Could you please explain this ?
The datasheets says VINLDO12 is used as a UVLO input. Also there are some versions of the chip with UVLO disabled ? Does this has any relation internally to the VINLDO12 leakage from 5V ? or it is mandatory to power it similar to AVDD or BUCK inputs.
Appreciate your quick reply
Thanks in advance
Regards
Abdu Samad