Other Parts Discussed in Thread: TINA-TI,
Tool/software: TINA-TI or Spice Models
Hi!
I have a problem with the LM3017. I want to do a Boost DC-DC covnerter with the following specifications:
- Vin=9,6..15
- Vout=48
- Ioutmax=0,83A
- Vout ripple=0,1
The designed converter needs the following values:
- Rfbb=1k
- Rfbt=36,8k
- L=42,6µ with a ripple current of 30%
- Rsen=20 m to limit the current to 1 A
- Co=111µ
- ESR(Co)=12m
- Rcomp=113k
- Ccomp=9,38p
- Ccomp2=18,3p
The pin EN/MODE I have powered with 2.1 V to work in BOOST mode.
I have done my circuit in Pspice and I have downloaded the model of LM3017 in the page of Texas Instruments.
The problem is that if I put the Vin higher than 12 V the system works well, but when I put the Vin lower than 12 V the Vout never reaches 48 V.
In this post I added an image of the simulation with an Iout of 0.5 A and Vin with 11V.
Thanks in advance
Regards
Adrian