This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25940: About way of thinking for leak current

Guru 19645 points
Part Number: TPS25940

Please let me know about determine Maximum Leak current below. 

①Datasheet page-6 is described Output leak current, but two ways; source and sink.

 Which spec is should reference?

②For example, source current is -2μA~2μA, maximum leak current is 4μA, is it correct?

Best regards,

Satoshi