Hi TI experts,
I have a thermostat project which leverages LMR16030 to provide outuput rated at 12V@2A. The input to LMR16030 is coming from AC line which is bridge rectified before feeding to the device. The issue I am observing is that audiable noise is generated while the device is output 12V@2A and or low load condition. Is there any recommendation on how to improve the audiable noise problem.? Peter3582.sch.pdf