Other Parts Discussed in Thread: TPS7B7702EVM
Hi,
I need some clarification on the TPS7B770x-Q1 antenna LDO :
When V Input (IN) is 0V :
Does the output pin is protected against Voltage VBattery ? Then what is the current going into the output pin
Same question when Vinput is 5V or 6V8
Does the Output pin is protected against VBat? What is the current going into the output pin (if there is some)
Thanks and regards,
Mohamed