Part Number: BQ24113EVM
Hi,
for battery charging prototype we're using BQ24113EVM.
Battery- Li-Ion 2-cell, System-Controlled Application.
the thing is- I'm connecting 2 lines to the MCU- STAT1 connected to microcontroller input, CMOD connected to microcontroller output
the PG# and CE# are don't care (CE# is always enabled, PG# line don't care).
Now- how it is exactly system-controlled? it's not specified in the datasheet.
I'll be glad to understand this part (remember, I'm using the EVM not the IC alone).
Regards