This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27520-G4: Some queries related to the TRM

Part Number: BQ27520-G4
Other Parts Discussed in Thread: BQSTUDIO

Hi,

In TRM it is mentioned "One cycle occurs when accumulated discharge ≥ CC Threshold."

1.What is mean by accumulated discharge?In bqstudio where can i find this value?

2.FCC=Qstart+PassedCharge+RM

In bqstudio where can i find Qstart value?

What is mean by passed charge?In bqstudio where can i find passed charge value?

Please see the attachment for various gauging parameter configurations.

Golden Gas Gauge File.docx 

In my battery it is marked as 3200 mAh.Maximum voltage is 4.2v.My system will work till 2.5v

I have done the charging and discharging using bqstudio and i faced some issues in the log datas

1.SOC is shown as 100 at Remaining capacity=2245,FCC=3250,voltage=4091mv,Full available capacity=2771,Nominal available capacity=1881.But to set the FC bit to set it takes around 3hrs(RM=3250,FCC=3250,Full available capacity=2471,Nominal available capacity=2471,Voltage=4162mv).Why this issue?How can i overcome this?

Expecting your valuable suggestions.....

Thanks,

Likhitha