This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Best solution for a Very low power PoE Class 1 device



Can you recommend the best PoE device to use for a Ultra Low Power Class 1 device, providing an output voltage between 3.0V and 3.3V with a max current of about 100mA.

There seems to be many devices to choose from, but all examples are given for 12W high power devices, and not specifically for the Class 1 which I assume could utilize smaller components and a much smaller isolated power transformer.


Any help with recommended devices and example circuits would be very welcome.