This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Product Selection Request



The circuit below is what I am trying to modify or replace.  Its purpose is to discharge voltage through a coil to generate an EMF.  I am using a 12VDC 3A Wall wort as a power supply.

Looking to purchase:  

     Transformer/Booster Module;   I would like to boost the voltage to 300-500VDC to charge a capacitor at a rate of 1-3 Hz.  Adjustable voltage if available.

     Capacitor;  Fast charge and discharge to maximize EMF in coil.

     Trigger Module;  Discharge capacitor at a rate of 1-3 Hz, adjustable if possible.  I would like to eliminate the flash tube.

I am interested in reducing individual components and replacing them with modular components.