Other Parts Discussed in Thread: CSD17483F4
Dear all,
I have a really strange problem with BQ24296 charger. It is used as charger only and charging currents required are up to 2 A. I can externally adjust charging current (regarding to undervoltage treshold) using additional transistor on Ilim, which works (I can switch between high/low charging current), but I have a very strange problem:
cell is charging also, when top voltage is reached or when module is in error mode (LED is blinking; i.e. I disconnect NTC). Actually, when the cell is empty, charging works ok. CC phase is finished, module goes to CV phase and also holds voltage at 4,207 V, but when the cell is full, charging still continues (current around 230 mA, LED goes off) as charger would go back to CC mode (without CV limit). The same happens, if I disconnect NTC and put module into error mode: "normal" charging is terminated and charging current goes to (around) 230 mA.
So, speaking simply, charger is charging the battery also when in error or overvoltage condition. How this can occur and how to avoid it?
Best regards,
Gregor
p.s. Test has been done without T2 as well, no changes. I2C is disconnected and nothing has been sent to chip.