This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5037: Half Bridge Topology

Part Number: LM5037

Hi,

My customer is considering to use the LM5037 as the half bridge driver.

However, the EVM of the LM5037 is nothing with the half bridge topology.

Is there any way to evaluate the LM5037 as the half bridge driver easily?

Best Regards,

Kuramochi

  • Kuramochi-san,

    I will have asked someone in the responsible product line to look into this and get back to you. You should get a reply in the next day or so.


    Thanks,
    Bernard
  • Hi Kuramochi-san,

    Unfortunatley there is no evm for the LM5037, the device is similar to the LM25037 which has an evm based on push-pull topology. You can directly replace the controller to evaluate the LM5037 on the LM25037EVAL. If you want to evalutate it based on half-bridge topology, you may need a lot of effects to put it on a half-bridge EVM such as LM5035CEVAL.

    Thanks
    Oliver